cancel
Showing results for 
Search instead for 
Did you mean: 

STM32WB55 Zigbee does not work

MT.2
Associate II

Hi there!

I have 2 STM32WB55 Nucleo boards, both of them are having the latest FUS and Zigbee FFD fw. However, one of them cannot run as normal(another goes vey well), after downloading Zigbee_OnOff_Server_Coord sample code to it, it shows the following error and LED1 to 3 on the Nucleo keep blinking one after the other. Could someone suggest why this happens and how to deal with this?

Cheers,

Mo

Error is shown via UART with 115200 as baud rate

[M4 APPLICATION] APP_ZIGBEE_Init

[M4 APPLICATION] **********************************************************

[M4 APPLICATION] WIRELESS COPROCESSOR FW:

[M4 APPLICATION] VERSION ID = 1.12.0

[M4 APPLICATION] **** Fatal error = ERROR Unknown (Err = 0)

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0