2024-07-17 03:43 AM
I am designing an Outdoor Radio product with STM32WLE5CBU6. my question is whether the Internal RC Oscillator is enough for my radio applications ? or do I need to add External TCXO in my circuit considering the outdoor temperature environment? for my product cost-cutting. please suggest.
Solved! Go to Solution.
2024-07-17 05:59 AM
It needs an external crystal to have wireless transmission capability.
2024-07-17 03:50 AM
@User16438042334827474767 wrote:my question is whether the Internal RC Oscillator is enough for my radio applications ?
Impossible to say without details of what these "radio applications" are.
You can find the specifications of the Internal RC Oscillator in the datasheet - work out from there whether that meets your requirements.
2024-07-17 03:54 AM
No.
Usually you want/need for GHz or many-MHz PLL a very stable clock source, typical a crystal.
See basic:
HSE32 is the "standard" clock for the PLL. (If 20 ct for a crystal is too much, you have another problem...)
2024-07-17 04:09 AM
Application LORA 868MHZ P2P Weather station.not LORAWAN.
2024-07-17 04:36 AM
Again, look at the specs in the datasheet - do they fit with your application requirements?
Local regulations will put requirements on frequency stability/accuracy ...
2024-07-17 05:23 AM
Ok, but you still want receive it - right ?
So:
The fequency should be, where you set it to - lets say- 0.01 MHz, 10kHz tolerance , to get it working at a channel bandwidth of 125 kHz.
THIS alone gives about 11 ppm max. tolerance, so even should be a +/- 10ppm crystal, not the cheapest 50ppm thing. And about the RC "reference" ...
... 10 000 ppm away .... you wouldnt even know, on which channel you sending.
...
2024-07-17 05:59 AM
It needs an external crystal to have wireless transmission capability.
2024-07-17 07:34 AM - edited 2024-07-17 07:34 AM
@User16438042334827474767 wrote:for my product cost-cutting. please suggest.
If you really want to cut costs, do you really need to use LoRa?
You pay a premium (to Semtech) for that ...
2024-07-20 05:57 AM - edited 2024-07-20 09:26 AM
Okay.