2023-03-31 06:40 AM
The steps performed:
2023-04-03 09:03 AM
Then am not able to read the FUS version..
2023-04-03 10:18 AM
Do you mean that you can read the FUS version via SWD and not via the USB interface?
Which version of CubeProgrammer are you using?
2023-04-05 10:58 PM
Do you mean that you can read the FUS version via SWD and not via the USB interface?
Exactly
Which version of CubeProgrammer are you using?
2.12.0
2023-04-05 11:14 PM
When I completely erase the chip and then tried to read the FUS version via USB still am not able to read FUS version
2023-04-06 12:12 AM - edited 2023-11-20 09:04 AM
As per STEP 4, the FUS version should have been read irrespective of anything, but when I erased the chip completely am not able to read the FUS version via USB.
2023-04-10 02:33 AM
Can anyone help me with the above-discussed ones?
2023-04-10 06:25 AM
Right now the chip has been erased completely.
Do you know how to enable the cortex M0+ before reading the FUS version via USB?
2023-04-10 06:28 AM
Or In other way of asking, Is there any way to start FUS without making the nswboot0 = 0 via USB?
2023-04-27 01:56 AM
Hello,
I tried to reproduce your issue, but I don't see it.
I'm using STM32CubeProgrammer v1.13.0.
Best Regards