2023-04-25 4:14 AM
I am trying to run BLE stack and VCP at the same time but when BLE stack run then VCP disables automatically.
Thank you in advance for reply.
2023-04-25 7:29 AM
+1
I have exactly the same problem right now. Everything is configured in CubeMX and
MX_USB_Device_Init();is called.
If I comment out
//MX_APPE_Init();the device is detected as CDC device on the PC.
But if STM32_WPAN is initialized (MX_APPE_Init(); called) the device is not detected as CDC device by the PC: "USB device not recognized"
Edit:
I have tried to narrow down the problem by comment out function calls:
MX_APPE_Init() -> appe_Tl_Init() -> TL_Init()If I comment out this line in tl_mbox.c, VCP is running (but BLE not):
TL_RefTable.p_device_info_table = &TL_DeviceInfoTable;Thanks! :full_moon_face:
2023-04-26 9:31 AM
Hello,
When you call VCP_Init function, a null pointer is give as second parameter, instead this null pointer, give a rx buffer in parameter like this:
VCP_Init( &VcpTxBuffer[0], &VcpRxBuffer[0] );And declare the rx buffer like this:
static uint8_t VcpRxBuffer[MAX_DBG_TRACE_MSG_SIZE]; /* Receive buffer over USB */Best Regards
2023-04-26 9:45 PM
Thank you Remy for reply
But in my code CubeMx didn't generate VCP_Init function it generates MX_USB_Device_Init function for usb device (CDC) for virtual com port.
2023-04-26 10:54 PM
hi BGeing.3
Just call this LL_HSEM_1StepLock( HSEM, 5 ); before calling MX_APPE_Init function.
2023-04-27 1:13 AM
Hello,
Sorry, I made a confusion, in your case you can look STM32WB-BLE-USB-CDC-VCOM example available on STM32 Hotspot GitHub. This example demonstrates how to use the BLE component alongside the USB peripheral for point-to-point communications. The application runs the BLE component as a GAP Peripheral and GATT Server, and the USB as a Device Communication Class (CDC), this is a typical application on how to use the STM32WBxx USB Device peripheral where the STM32WB MCU behaves as a USB-to-RS232 bridge following the Virtual COM Port (VCP) implementation.
In AN5289 on figure 9, there is a description that show how to use USB on CPU1 because the USB and RNG IPs share the same source clock, so you should manage semaphore.
Best Regards
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.