2024-12-16 9:08 AM - last edited on 2025-01-14 3:02 AM by STTwo-32
I am trying to communicate with ADS1115 using Seeed Studio's LoRa Wio E5 mini in the I2C2 peripheral to which PA15 and PB15 are connected. It doesn't work and I am able to see nothing on my logic analyzer. SCL stays high and SCL stays low with no data at all in the bus. I have enabled pull up resistors for the I2C pins in my Wio E5 mini using CubeMX. I am using Seeed Studio LoRaWan for the LoRaWan stack to connect to my TTN network and without the I2C master transmit or device ready commands the demo code runs well and I receive the dummy data at TTN side. If I include any master transmit or any command related to I2C the code gets stuck at MX_LoRaWAN_Init().
Solved! Go to Solution.
2025-01-14 3:25 AM
Hello @user_01
For the component you are using, is a third-party product based on the STM32WLE MCU. So, it will be a very good idea to look for an answer on the forum of our third-party. I think you have already found a solution here.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-01-14 3:25 AM
Hello @user_01
For the component you are using, is a third-party product based on the STM32WLE MCU. So, it will be a very good idea to look for an answer on the forum of our third-party. I think you have already found a solution here.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.