2018-09-20 7:00 AM
Hi,
I have two boards that I would like to use with the I-NUCLEO-LRWAN1 expansion board:
NUCLEO-F411RE and NUCLEO-L152RE.
Is any of them compatible with I-NUCLEO-LRWAN1?
Thanks.
2018-09-20 7:57 AM
Hello @DB.7lendea ,
Yes, these boards are compatible with I-NUCLEO-LRWAN1.
You can check the compatible products and softwares on the board page:
https://www.st.com/en/evaluation-tools/nucleo-f411re.html
https://www.st.com/en/evaluation-tools/nucleo-l152re.html
With Regards,
Imen
2018-09-20 8:14 AM
You're talking through the USART on D0/D1 of the shield, I don't think NUCLEO-64 boards are ideal for that as you have some clashing with the VCP, but you should be able to resolve with SB (solder bridges) changes.
The NUCLEO-144 or DISCO boards with shield would be arguably better choices.
2018-09-21 12:17 AM
Ok, noted.
Thanks.
2018-09-21 6:50 AM
Hmm,
I see in the technical documentation for the I-CUBE-LRWAN software, only the following boards are supported:
NUCLEO-L053R8
NUCLEO-L073RZ
NUCLEO-L152RE
NUCLEO-L476RG
Do I need to make some changes in the software to be able to use the F411RE board?