Skip to main content
Associate II
Nov 19, 2024 9:45 AM UTC
Solved

STM32H747I-DISCO QT

Hi,

I have a question regarding the implementation of the Qt framework for the STM32H747I-DISCO board. While browsing the Qt website, I noticed an example for the similar STM32H750B-DK board, but I couldn’t find any information specific to the DISCO model. So my question is: will the Qt implementation for the 750B board be compatible with the 747 board? Will it be possible to run the sample applications on both boards without any modifications?

I have another question. From what I understand, it is necessary to use a bootloader (due to the small flash memory). Is it possible to access the bootloader code through STM32Cube/gitrepo? And will it be available for the 747 board? (I saw that a HEX file is uploaded on the website.)

Thank you in advance for your response.
Rafał

This topic has been closed for replies.
mƎALLEm
mƎALLEmBest answer
ST Technical Moderator
Nov 19, 2024 9:59 AM UTC

Sorry I misunderstood your question.


@RafalBil wrote:

but from what I understand, ST doesn't officially support it. Would it be better if I asked on the QT forum?


Yes, as I said QT is not the frame work of ST. ST only supports TouchGFX.


@RafalBil wrote:

 Would it be better if I asked on the QT forum?


Indeed. In that case you need to contact them directly: https://www.qt.io/contact-us.

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.

4 replies

mƎALLEm
ST Technical Moderator
Nov 19, 2024 9:52 AM UTC

Hello @RafalBil ,

QT is not a ST development platform. But according to this link  STM32H750B-DK board is supported.

Hope I answered your question.

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
RafalBilAuthor
Associate II
Nov 19, 2024 9:56 AM UTC

Thanks, from what I noticed, the 750B is supported. I'm wondering if QT will be compatible with the 747, but from what I understand, ST doesn't officially support it. Would it be better if I asked on the QT forum?

mƎALLEm
mƎALLEmBest answer
ST Technical Moderator
Nov 19, 2024 9:59 AM UTC

Sorry I misunderstood your question.


@RafalBil wrote:

but from what I understand, ST doesn't officially support it. Would it be better if I asked on the QT forum?


Yes, as I said QT is not the frame work of ST. ST only supports TouchGFX.


@RafalBil wrote:

 Would it be better if I asked on the QT forum?


Indeed. In that case you need to contact them directly: https://www.qt.io/contact-us.

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
Andrew Neil
Super User
Nov 19, 2024 10:43 AM UTC
A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.