2024-07-16 06:28 PM
There doesn't seem to be any project in the whole STM32CubeWB package that uses the HSE with PLL. At least I couldn't find any with a .IOC file. Most samples in the package use the MSI clock, except, of course, for the wireless projects that use HSE for better accuracy. But in all those projects that use the HSE, they use the clock directly, not through the PLL, and then they clock the main CPU at 32 MHz, not at 64 MHz.
Of course it is possible to modify the configuration to use the HSE with the PLL. But it is rather strange that with all the projects in the package, everyone that do use the HSE, doesn't use the PLL and chooses to configure the CPU at a lower frequency. To be honest, it makes one suspicious that it could be a problem and it might not work reliably if one try to use the HSE with the PLL.
Anybody has any actual experience with a wireless project using the HSE and clocking the CPU at 64 MHz through the PLL?
Thanks