2022-04-25 1:48 PM
I'm designing multichannel ADC using scan conversion mode.
Using HAL_ADC_Start_DMA code, the 1~9 ADC is easily saved in the DMA but. from 10, the ADC is not working and I cannot see any UART communication data.
How to use ADC channel 10~16 in the Nucleo-WB55 board or is there anything I missed?
In addition, is there any exam sending the row data from the WB55 board to the PC through Bluetooth?
here is the code.
#include "main.h"
#include "stm32_seq.h"
#include "string.h"
#include "stdio.h"
ADC_HandleTypeDef hadc1;
DMA_HandleTypeDef hdma_adc1;
HAL_StatusTypeDef ret;
UART_HandleTypeDef huart1;
ADC_ChannelConfTypeDef sConfig;
float value[16];
uint16_t DMA_value[16];
int main(void)
{
HAL_Init();
MX_APPE_Config();
SystemClock_Config();
PeriphCommonClock_Config();
MX_IPCC_Init();
MX_GPIO_Init();
MX_DMA_Init();
MX_RF_Init();
MX_RTC_Init();
MX_USB_PCD_Init();
MX_ADC1_Init();
MX_APPE_Init();
MX_APPE_Process();
HAL_ADC_Start_DMA(&hadc1,(uint32_t*)DMA_value, 16);
while (1)
{
HAL_ADC_Start(&hadc1);
HAL_Delay(100);
printf("%.d\t %.d\t %.d\t %.d\t %.d\t %.d\t %.d\t %.d\t %.d\t %.d\t %.d\t %.d\t %.d\t %.d\t %.d\t %.d\t \r\n", DMA_value[0],DMA_value[1],DMA_value[2],DMA_value[3],DMA_value[4],DMA_value[5],DMA_value[6],DMA_value[7],DMA_value[8],DMA_value[9],DMA_value[10],DMA_value[11],DMA_value[12],DMA_value[13],DMA_value[14],DMA_value[15]);
fflush(stdout);
}
}
static void MX_ADC1_Init(void)
{
hadc1.Instance = ADC1;
hadc1.Init.ClockPrescaler = ADC_CLOCK_ASYNC_DIV1;
hadc1.Init.Resolution = ADC_RESOLUTION_12B;
hadc1.Init.DataAlign = ADC_DATAALIGN_RIGHT;
hadc1.Init.ScanConvMode = ADC_SCAN_ENABLE;
hadc1.Init.EOCSelection = ADC_EOC_SINGLE_CONV;
hadc1.Init.LowPowerAutoWait = DISABLE;
hadc1.Init.ContinuousConvMode = DISABLE;
hadc1.Init.NbrOfConversion = 15;
hadc1.Init.DiscontinuousConvMode = DISABLE;
hadc1.Init.ExternalTrigConv = ADC_SOFTWARE_START;
hadc1.Init.ExternalTrigConvEdge = ADC_EXTERNALTRIGCONVEDGE_NONE;
hadc1.Init.DMAContinuousRequests = ENABLE;
hadc1.Init.Overrun = ADC_OVR_DATA_PRESERVED;
hadc1.Init.OversamplingMode = ENABLE;
hadc1.Init.Oversampling.Ratio = ADC_OVERSAMPLING_RATIO_256;
hadc1.Init.Oversampling.RightBitShift = ADC_RIGHTBITSHIFT_4;
hadc1.Init.Oversampling.TriggeredMode = ADC_TRIGGEREDMODE_SINGLE_TRIGGER;
hadc1.Init.Oversampling.OversamplingStopReset = ADC_REGOVERSAMPLING_CONTINUED_MODE;
if (HAL_ADC_Init(&hadc1) != HAL_OK)
{
Error_Handler();
}
sConfig.Channel = ADC_CHANNEL_1;
sConfig.Rank = ADC_REGULAR_RANK_1;
sConfig.SamplingTime = ADC_SAMPLETIME_47CYCLES_5;
sConfig.SingleDiff = ADC_SINGLE_ENDED;
sConfig.OffsetNumber = ADC_OFFSET_NONE;
sConfig.Offset = 0;
if (HAL_ADC_ConfigChannel(&hadc1, &sConfig) != HAL_OK)
{
Error_Handler();
}
sConfig.Channel = ADC_CHANNEL_2;
sConfig.Rank = ADC_REGULAR_RANK_2;
if (HAL_ADC_ConfigChannel(&hadc1, &sConfig) != HAL_OK)
{
Error_Handler();
}
sConfig.Channel = ADC_CHANNEL_3;
sConfig.Rank = ADC_REGULAR_RANK_3;
if (HAL_ADC_ConfigChannel(&hadc1, &sConfig) != HAL_OK)
{
Error_Handler();
}
sConfig.Channel = ADC_CHANNEL_4;
sConfig.Rank = ADC_REGULAR_RANK_4;
if (HAL_ADC_ConfigChannel(&hadc1, &sConfig) != HAL_OK)
{
Error_Handler();
}
sConfig.Channel = ADC_CHANNEL_5;
sConfig.Rank = ADC_REGULAR_RANK_5;
if (HAL_ADC_ConfigChannel(&hadc1, &sConfig) != HAL_OK)
{
Error_Handler();
}
sConfig.Channel = ADC_CHANNEL_6;
sConfig.Rank = ADC_REGULAR_RANK_6;
if (HAL_ADC_ConfigChannel(&hadc1, &sConfig) != HAL_OK)
{
Error_Handler();
}
sConfig.Channel = ADC_CHANNEL_7;
sConfig.Rank = ADC_REGULAR_RANK_7;
if (HAL_ADC_ConfigChannel(&hadc1, &sConfig) != HAL_OK)
{
Error_Handler();
}
sConfig.Channel = ADC_CHANNEL_8;
sConfig.Rank = ADC_REGULAR_RANK_8;
if (HAL_ADC_ConfigChannel(&hadc1, &sConfig) != HAL_OK)
{
Error_Handler();
}
sConfig.Channel = ADC_CHANNEL_9;
sConfig.Rank = ADC_REGULAR_RANK_9;
if (HAL_ADC_ConfigChannel(&hadc1, &sConfig) != HAL_OK)
{
Error_Handler();
}
sConfig.Channel = ADC_CHANNEL_10;
sConfig.Rank = ADC_REGULAR_RANK_10;
if (HAL_ADC_ConfigChannel(&hadc1, &sConfig) != HAL_OK)
{
Error_Handler();
}
}
2022-04-25 5:37 PM
> sConfig.Channel = ADC_CHANNEL_10;
> sConfig.Rank = ADC_REGULAR_RANK_10;
Looks like your code is only initializing 10 channels. To use more than 10 channels, you will need to initialize the other in a similar fashion to the first 10.
2022-05-04 12:40 PM
this problem is solved by using STM32CubeMX. I think the previous setting has something wrong. Now all 16 channel works successfully and I can save them into the DMA.