2024-02-22 02:27 AM
Hi,
I want to know how to transmit data in ble for the interval of 10ms and How do I can change the ticks to achieve it.
Thanks and Regards,
LR.2
2024-04-15 07:51 AM
Hello @LR.2
What I suggest you take a look at the BLE_Heart_Rate example and try to understand how the data sending is working. Then, you can use the same procedure and change the timing parameters.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.