2020-08-04 7:56 AM
Just like communicating with a Bluetooth sensor (HC-06) via USART, can I transfer an SPI camera image to an iOS or Android based device via BLE?
2020-08-04 8:21 AM
Yes you can use an SPI camara module connected to the STM32WB device to capture the video data and transfer it to a mobile application via BLE.
We made such demo and it works pretty well but does not exceed 5 to 10 frames per second depending on the picture resolution.
You may even add an audio part with an external microphone connected to the STMWB through the SAI interface.
2020-08-04 9:49 AM
Hi Remi,
Can I use USART to send data with BLE, if not, can you give me a brief explanation about communication?
How should I search to see related documentation about it?
Thanks.
2020-10-25 4:47 PM
What example would this be found in?