2020-01-24 3:35 AM
Hi,
I am using B-L072Z-LRWAN1 discovery kit. I want to implement USB-CDC functionality for my project.
I created the project using STM32CubeMX with the settings of USB-CDC after following this STM USB training link
https://www.youtube.com/watch?v=h9T0RTu9Muc&list=PLnMKNibPkDnFFRBVD206EfnnHhQZI4Hxa&index=9
After that i connected one USB to CN7 connector and run the code in debugging mode. Then i connected another USB to CN11 connector which is USER USB.
As per the video,
USB connected to CN7 should show one COM port with name "STMicroelectronics STLink VCP"
USB connected to CN11 should show another COM port with name "STMicroelectronics VCP".
But after connecting i am not detecting 2nd com port on my PC side in short no virtual port is showing after connecting to USER USB connector.
Please guide me regarding this with any example related to the same controller or any hardware settings need to be done for its working.
Thanks
Shubham
2020-01-27 9:29 PM
you can find not similar but project for another controller on your IDE folder
2020-01-28 8:58 PM
Ya followed that but still facing problem. Till now i have tried following things:-
/* Enable HSI Oscillator to be used as System clock source
Enable HSI48 Oscillator to be used as USB clock source */
RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI | RCC_OSCILLATORTYPE_HSI48;
RCC_OscInitStruct.HSIState = RCC_HSI_ON;
RCC_OscInitStruct.HSI48State = RCC_HSI48_ON;
HAL_RCC_OscConfig(&RCC_OscInitStruct);
/* Select HSI48 as USB clock source */
PeriphClkInitStruct.PeriphClockSelection = RCC_PERIPHCLK_USB;
PeriphClkInitStruct.UsbClockSelection = RCC_USBCLKSOURCE_HSI48;
HAL_RCCEx_PeriphCLKConfig(&PeriphClkInitStruct);
/* Select HSI as system clock source and configure the HCLK, PCLK1 and PCLK2
clock dividers */
RCC_ClkInitStruct.ClockType = (RCC_CLOCKTYPE_SYSCLK | RCC_CLOCKTYPE_HCLK | RCC_CLOCKTYPE_PCLK1 | RCC_CLOCKTYPE_PCLK2);
RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_HSI;
RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV1;
RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV1;
HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_0);
/*Configure the clock recovery system (CRS)**********************************/
/*Enable CRS Clock*/
__HAL_RCC_CRS_CLK_ENABLE();
/* Default Synchro Signal division factor (not divided) */
RCC_CRSInitStruct.Prescaler = RCC_CRS_SYNC_DIV1;
/* Set the SYNCSRC[1:0] bits according to CRS_Source value */
RCC_CRSInitStruct.Source = RCC_CRS_SYNC_SOURCE_USB;
/* HSI48 is synchronized with USB SOF at 1KHz rate */
RCC_CRSInitStruct.ReloadValue = __HAL_RCC_CRS_RELOADVALUE_CALCULATE(48000000, 1000);
RCC_CRSInitStruct.ErrorLimitValue = RCC_CRS_ERRORLIMIT_DEFAULT;
/* Set the TRIM[5:0] to the default value*/
RCC_CRSInitStruct.HSI48CalibrationValue = 0x20;
/* Start automatic synchronization */
HAL_RCCEx_CRSConfig (&RCC_CRSInitStruct);
2020-01-29 2:04 PM
I've had the USB working on the Murata modules, for the DISCO board I recall there being Solder Bridges (SB) that you must attend too. Review schematic/user manual.
2020-01-30 4:20 AM
Hi clive1,
Yes that i already done.
Anyways i was able to resolve the issue. I did the following things t o resolve the issue:-
2020-03-23 6:00 AM
Hello,
I intend to add USB CDC feature on the current PING PONG project on my B-L072Z-LRWAN board.
First I did the solder bridges configurations presented on this thread.
Then, I created a simple STM32Cube project for this board, configuring USB CDC. It worked correctly. But it doesn't have the LoraWan stack and porting it to a Cube Project is not a simple task (I tried it, without success). But, I could see USB CDC working.
To add USB CDC on the PingPong project, I got the project from STM32L073Z_EVAL and added the features to PingPong project. But it is not working. My PC cannot recognize the USB port.
I set 0x1000 heap size at linker script.
Below my system clock configuration:
void SystemClock_Config(void)
{
RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};
RCC_OscInitTypeDef RCC_OscInitStruct = {0};
RCC_PeriphCLKInitTypeDef PeriphClkInitStruct = {0};
/* Enable HSE Oscillator and Activate PLL with HSE as source */
RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI;
RCC_OscInitStruct.HSEState = RCC_HSE_OFF;
RCC_OscInitStruct.HSIState = RCC_HSI_ON;
RCC_OscInitStruct.HSICalibrationValue = RCC_HSICALIBRATION_DEFAULT;
RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSI;
RCC_OscInitStruct.PLL.PLLMUL = RCC_PLLMUL_6;
RCC_OscInitStruct.PLL.PLLDIV = RCC_PLLDIV_3;
if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
{
Error_Handler();
}
/*Select PLL 48 MHz output as USB clock source */
PeriphClkInitStruct.PeriphClockSelection = RCC_PERIPHCLK_USB;
PeriphClkInitStruct.UsbClockSelection = RCC_USBCLKSOURCE_PLL;
HAL_RCCEx_PeriphCLKConfig(&PeriphClkInitStruct);
/* Set Voltage scale1 as MCU will run at 32MHz */
__HAL_RCC_PWR_CLK_ENABLE();
__HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE1);
/* Poll VOSF bit of in PWR_CSR. Wait until it is reset to 0 */
while (__HAL_PWR_GET_FLAG(PWR_FLAG_VOS) != RESET) {};
/* Select PLL as system clock source and configure the HCLK, PCLK1 and PCLK2
clocks dividers */
RCC_ClkInitStruct.ClockType = (RCC_CLOCKTYPE_SYSCLK | RCC_CLOCKTYPE_HCLK | RCC_CLOCKTYPE_PCLK1 | RCC_CLOCKTYPE_PCLK2);
RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;
RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV1;
RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV1;
if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_1) != HAL_OK)
{
Error_Handler();
}
}
Could you please advise me where am I doing wrong ... or how should I debug my implementation?]
Best regards,
Flavio
2023-02-08 2:09 AM
Solder the connections SB16 and SB15, by default board comes with open line USB_DM and USB_DP. Once you short SB16 and SB15 you will find another virtual com port.