2024-07-22 11:59 PM - edited 2024-07-23 12:00 AM
Hello,
I am developing a BLE HID device using the STM32WB55.
I am generating random static addresses using a program implemented in the STM32CubeWB. This is used to identify multiple peripherals with the same functionality.
#else
/* Get RNG semaphore */
while(LL_HSEM_1StepLock(HSEM, CFG_HW_RNG_SEMID));
/* Enable RNG */
__HAL_RNG_ENABLE(&hrng);
/* Enable HSI48 oscillator */
LL_RCC_HSI48_Enable();
/* Wait until HSI48 is ready */
while(! LL_RCC_HSI48_IsReady());
if (HAL_RNG_GenerateRandomNumber(&hrng, &a_srd_bd_addr[1]) != HAL_OK)
{
/* Random number generation error */
Error_Handler();
}
if (HAL_RNG_GenerateRandomNumber(&hrng, &a_srd_bd_addr[0]) != HAL_OK)
{
/* Random number generation error */
Error_Handler();
}
a_srd_bd_addr[1] |= 0xC000; /* The two upper bits shall be set to 1 */
/* Disable HSI48 oscillator */
LL_RCC_HSI48_Disable();
/* Disable RNG */
__HAL_RNG_DISABLE(&hrng);
/* Release RNG semaphore */
LL_HSEM_ReleaseLock(HSEM, CFG_HW_RNG_SEMID, 0);
#endif /* CFG_STATIC_RANDOM_ADDRESS */
#if (CFG_BLE_ADDRESS_TYPE != GAP_PUBLIC_ADDR)
ret = aci_hal_write_config_data(CONFIG_DATA_RANDOM_ADDRESS_OFFSET, CONFIG_DATA_RANDOM_ADDRESS_LEN, (uint8_t*)a_srd_bd_addr);
if (ret != BLE_STATUS_SUCCESS)
{
APP_DBG_MSG(" Fail : aci_hal_write_config_data command - CONFIG_DATA_RANDOM_ADDRESS_OFFSET, result: 0x%x \n", ret);
}
else
{
APP_DBG_MSG(" Success: aci_hal_write_config_data command - CONFIG_DATA_RANDOM_ADDRESS_OFFSET\n");
APP_DBG_MSG(" Random Bluetooth Address: %02x:%02x:%02x:%02x:%02x:%02x\n", (uint8_t)(a_srd_bd_addr[1] >> 8),
(uint8_t)(a_srd_bd_addr[1]),
(uint8_t)(a_srd_bd_addr[0] >> 24),
(uint8_t)(a_srd_bd_addr[0] >> 16),
(uint8_t)(a_srd_bd_addr[0] >> 8),
(uint8_t)(a_srd_bd_addr[0]));
}
#endif /* CFG_BLE_ADDRESS_TYPE != GAP_PUBLIC_ADDR */
Is there any way to restore the address generated here after a reset?
This is to perform a reconnection of the coupled device using ADV_DIRECT_IND with the restored random address.
I thought of saving it to NVM as a method, is it possible?
I would appreciate if you could answer me.
Best regards.
2024-07-23 5:45 AM
If your intention is to generate a unique number to identify the device, I suggest using what's already onboard for that. The UID64 register value is guaranteed unique for each device.
Barring that, there certainly are ways to save information. Saving to a flash sector can work, as can saving to SRAM if power is not lost.
2024-07-24 1:04 AM
Hello. @TDK
Thank you for your reply.
Thanks to you I have a better understanding of UID.
This time, however, I would like to add a process to change the random static address when a new connection is initiated after this (pressing the pairing button again during pairing).
Therefore, I don't think UID can be used only for identification (not sure if this is correct, sorry).
I'll think about how and when to save it to flash some more. Thanks.
Best regards.
2024-08-26 7:29 AM
Hello @ELEHM
Could you please give more details about your use case and what do you exactly want to change.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-09-23 7:17 PM
Hello @STTwo-32
Sorry for the late reply.
Here is what I would like to do
--------------------------------------------------------------------------------------------------------------------
1. save the address and key for encryption when connecting (even after power off).
2. after power is restored, try to connect to the original connection point with ADV_DIRECT_IND (if not possible, do nothing)
3. if the pairing button is pressed, a new address is generated and advertised with ADV_IND.
--------------------------------------------------------------------------------------------------------------------
Also, if you have multiple boards, you want to identify each board.
Best Regards.