Skip to main content
DTayl.4
Visitor II
June 6, 2022
Question

How do I properly load I-CUBE-LRWAN into STM32CubeIDE? I have tried importing filesystem projects from various levels of the I-CUBE-LRWAN hierarchy but I'm not convinced I'm getting it right.

  • June 6, 2022
  • 1 reply
  • 1186 views

Say I want the Projects/B-L072Z-LRWAN1/Applications/LoRaWAN/LoRaWAN_AT_Slave project loaded up.

What exactly am I supposed to do in the IDE?

I've loaded that project up, but can only build the debug configuration - it doesn't seem right.

I did change the code to use AS923 and also added an extra message to the startup and those changes seem to be present on my board but I can't believe I have the project imported properly.

I'm also wondering how I use the LoRaWAN code for my own project. Am I supposed to import either the AT or End_Node project and start adding my code to them?

This topic has been closed for replies.

1 reply

Avan .12
Associate II
March 26, 2023

you have to import it as an existing project into STM32CubeIDE.

check out https://youtu.be/M1NZ61CAU0I