2023-01-22 11:21 PM
2023-01-23 1:56 AM
Hello @AJAY S ,
The MAX30102 operates on a single 1.8V power supply and a separate 3.3V power supply for the internal LEDs. (DATASHEET)
So, try to provide 1V8 as a power supply for the sensor MAX30102.
Foued
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2023-01-23 2:11 AM
this is my shematic design sir here i2c i use 1v8 is that okey to communicate STM32WBMMG chip. in between 3v3 to 1v8 level shifter is required? or not thats my doubt
2023-01-23 2:40 AM
I think you are alright as recommended in the Datasheet of the sensor MAX30102 :
Foued
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2023-01-23 2:42 AM
MY host is 3V3 sir,but my sensor is 1v8 thats why i had confussion.
2023-01-23 2:50 AM
Try to use a regulator to provide 1V8 like the LDK130M-R.
I advice you take a look : Schematic diagram Motion MEMS and environmental sensor expansion board for STM32 Nucleo -
When your question is answered, please close this topic by choosing Select as Best. This will help other users find that answer faster.
Foued
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2023-01-23 4:40 AM
You can use it , because is in max ratings but need have this levels in range primary low under ...as you see High dont have defined up limit ... abs max ratings is 6V
2023-01-23 9:46 PM
thank you for your support
2023-01-28 2:48 AM
@AJAY S please help me regarding the programming of this mcu stm32wbmmg i am able to flash a program but not able to find out the ble module
2023-01-28 4:27 AM