2023-12-04 05:39 AM
Hi All!
We have a requirement to disable OTA updates either via hardware or by settings a fuse, this is due to the need for a low-maintaince, low-complexity, high-security method to prevent updates to those without physical access to the device.
Is there a fuse or fuses that can be used for this purpose? Or maybe a PIN that can be used for this?
We're looking to disable the OTA (aka FUOTA) for the STM32WLE5CBU6 which is listed as OTA capable in the datasheet.
Thanks all! :D
Solved! Go to Solution.
2024-06-20 03:18 AM
Hello @billyjoel
There is no way to do that. FUOTA is purely software and does not check hardware settings.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-06-20 03:18 AM
Hello @billyjoel
There is no way to do that. FUOTA is purely software and does not check hardware settings.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.