cancel
Showing results for 
Search instead for 
Did you mean: 

GMSK RX/TX

MCarl.7
Associate II

In this doc searching for the keyword MSK I come across the following:

"MSK and GMSK RX/TX with BR from 1.2 to 300 Kbit/s and TX only with BR from 0.1 to 1.2 Kbit/s"

"The (G)MSK and BPSK modems only supports transmission"

"The FSK modem with a bit rate above 1.2 kbps and a frequency deviation equal to a quarter of the bit rate, allows the MSK modulation to be used in both receive and transmit."

" This MSK modulation is only available in transmit mode"

The question is can I use GMSK for receive?

1 REPLY 1
MCarl.7
Associate II

Ok. clear with the text saying:

"a. The (G)FSK modem can be used for (G)MSK modulation when setting the frequency deviation to a quarter of the bit rate"