cancel
Showing results for 
Search instead for 
Did you mean: 

Receive sensitivity of GFSK modem on STM32WL55

MoralkaraLynn
Associate

The STM32WL5x Datasheet mentions the RX Sensitivity of the Radio Modem for both 2-FSK and LoRa modulation (see image below) but makes no mention of GFSK, GMSK or BPSK

MoralkaraLynn_0-1725865626245.png

What are the receive sensitivity values for these modulation schemes?

1 ACCEPTED SOLUTION

Accepted Solutions
STTwo-32
ST Employee

Hello @MoralkaraLynn and welcome to the ST Community .

The sub-GHz radio implemented on the STM32WL5x support Transmission and Reception using the LoRa and the 2-FSK modulations. But it supports only the Transmission for the 2-MSK and BPSK modulation. So, no reception for GMSK, MSK and BPSK. For the GFSK, it is mentioned on the 2-FSK (FSK & GFSK). 

Then, RX sensitivity parameter should be available only For LoRa, FSK and GFSK.

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

1 REPLY 1
STTwo-32
ST Employee

Hello @MoralkaraLynn and welcome to the ST Community .

The sub-GHz radio implemented on the STM32WL5x support Transmission and Reception using the LoRa and the 2-FSK modulations. But it supports only the Transmission for the 2-MSK and BPSK modulation. So, no reception for GMSK, MSK and BPSK. For the GFSK, it is mentioned on the 2-FSK (FSK & GFSK). 

Then, RX sensitivity parameter should be available only For LoRa, FSK and GFSK.

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.