User Activity

Hi,Is there any side effects of changing the RF Frequency of the Lora Modem during runtime.Radio.SetChannel(RF_FREQUENCY);Can this be used to change the frequency at runtime? Thanks
Hi,I have designed two PCBs that use STM32WLE5C8U6. I am experiencing range problems. The communications does not exceed 15 meters of range. What is the expected range? Below is what I use to initialize the radio. I have an R0 so that I switch betwee...
In this doc searching for the keyword MSK I come across the following:"MSK and GMSK RX/TX with BR from 1.2 to 300 Kbit/s and TX only with BR from 0.1 to 1.2 Kbit/s""The (G)MSK and BPSK modems only supports transmission""The FSK modem with a bit rate ...