cancel
Showing results for 
Search instead for 
Did you mean: 

FreeRTOS osThreadFlagsWait can return osErrorTimeout early

Graham1
Associate II

I have come across an issue which I believe is a bug in the implementation of the osThreadFlagsWait function.

Scenario

A thread is waiting on a flag (e.g. 0x2u) for a timeout above 0, before this timeout should occur, there are multiple other flags set on the thread (e.g. 0x1u) using osThreadFlagsSet, this results in the osThreadFlagsWait function returning with a value of osErrorTimeout sooner than the set timeout.

Cause

The xTaskNotifyWait function which is called by osThreadFlagsWait returns each time the 0x1u flag is set, resulting in this section of code being run:

Graham1_1-1738260906062.png

Note that t0 is set to the return value of xTaskGetTickCount() at the start of the wait loop, so is the start time, tout is a timeout value passed to xTaskNotifyWait, which is originally the set timeout, but is adjusted each time the xTaskNotifyWait function returns.

The issue with the code above is that the value of td is the total time that the thread has been waiting, this is subtracting from tout each time a flag is set that is not waited on e.g.

for a set timeout of 100, if the flag that is not waited on happens every 10 ticks, the value of td and tout will be as follows for each time xTaskNotifyWait returns:

  1. td = 10 therefore tout = (100 - 10) = 90
  2. td = 20 therefore tout = (90 - 20) = 70
  3. td = 30 therefore tout = (70 - 30) = 40
  4. td = 40 therefore tout = (40 - 40) = 0 // timeout is detected on the next call to xTaskNotifyWait

This gives a timeout of 40 ticks in this case instead of the desired 100.

Suggested Fix

To fix this issue, I would suggest removing the cumulative subtraction from tout, instead replacing it with a subtraction of td from the set timeout e.g.

Graham1_2-1738261376861.png

 

4 REPLIES 4
TDK
Super User

The code on GitHub already has this change.

stm32-mw-freertos/Source/CMSIS_RTOS_V2/cmsis_os2.c at e41c220a37adbb55b59dca704def6e73d6258b95 · STMicroelectronics/stm32-mw-freertos

 

What exact chip and library are you using? Are you using the latest version?

 

If you have an IOC file that generates the faulty code please attach it.

If you feel a post has answered your question, please click "Accept as Solution".

I am using an STM32WB55, using the FREERTOS middleware from STM32CubeIDEs Pinout & configuration tool with repository version STM32Cube_FW_WB_V1.21.0 which I believe is the latest.

 

https://github.com/STMicroelectronics/STM32CubeWB/blob/dcc538339a30165ced95745969706b7423e3d96d/Middlewares/Third_Party/FreeRTOS/Source/CMSIS_RTOS_V2/cmsis_os2.c#L862

STTwo-32
ST Employee

Hello @Graham1 @TDK 

Thank you so much for bringing this on the ST Community. I've escalated for review on the Future (under internal ticket number (204574).

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.