User Activity

We have a device which connects to two other devices as a central, and also is connected to by a third device (Mobile Phone) as a peripheral.When updating the Bluetooth firmware binary from version 1.20.0 to 1.21.0 we have started experiencing discon...
I have come across an issue which I believe is a bug in the implementation of the osThreadFlagsWait function.ScenarioA thread is waiting on a flag (e.g. 0x2u) for a timeout above 0, before this timeout should occur, there are multiple other flags set...
While attempting to identify an issue with reading and writing to emulated EEPROM, I have identified a bug in V7.0.0 of the X-CUBE-EEPROM source code.This was identified in the STM32WB version of `flash_interface.c` with `DUALCORE_FLASH_SHARING` defi...
Hey everyone, I am trying to send out two different characteristic notifications, one after the other and I am getting error 0x93 (BLE_STATUS_BUSY) in return for the second characteristic update, It then takes at least 100mS (often a lot more than th...
Kudos from