2023-10-11 7:19 AM
Hello,
I am using the STM32WL55 with the BLUENRG-2N.
i need to add the Firmware update OTA capability using the Bluetooth (BLUENRG-2N)
the examples of FUOTA for STM32WL are based on LoraWAN protocol ... so it is not what i looking for.
Do you have any examples or documentation (application note or ...) that can help me to make my application ?
Thank you,
Sincerely.
Solved! Go to Solution.
2024-05-16 2:29 AM
i have make finally my custom bootloader.
the entry point of the code is the bootloader (CM4 only),
if there is new app on the eeprom, the code jump to the existing app on the flash (executing CM4 and CM0PLUS)
the application (in CM0PLUS) receive the new fw by Bluetooth with the BlueNRG-2 and save it on the EEPROME (for booth cores)
then the app jump to the bootloader again to download the new firmware from the eeprom to the flash
2023-11-23 1:05 AM - edited 2023-11-23 1:09 AM
Hello @malarab
I suggest you to take a look at the AN4869 and AN5463. they may help you.
PS: STM32WL and BlueNRG-2 are using different technologies.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-05-16 2:29 AM
i have make finally my custom bootloader.
the entry point of the code is the bootloader (CM4 only),
if there is new app on the eeprom, the code jump to the existing app on the flash (executing CM4 and CM0PLUS)
the application (in CM0PLUS) receive the new fw by Bluetooth with the BlueNRG-2 and save it on the EEPROME (for booth cores)
then the app jump to the bootloader again to download the new firmware from the eeprom to the flash
2024-07-16 5:06 AM - edited 2024-07-17 6:32 AM
Hello @malarab
I am in the same situation as you, the only difference is thaht I used an STM32F4xx, I'd like to know if do you provide maybe a github or something like that of you project? Or maybe give me some guidelines.
Thanks
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.