2024-03-25 10:05 PM
Hello, I am developing a device using STM32WL chipset.
I'm currently taking the FCC certification test, but it failed in R.S.E (Radio spurious emmision), so I've been reviewing it for 3 weeks.
There was an FCC certification logo on the STM32WL Ev-kit, so I searched for the FCC ID and found a test report like the attached file.
If you look at page 23, it says "Final measurement detector: CISPR Average". Is the AVG value measured by CISPR correct?
The device we are developing is in a situation where Peak passes in the FCC R.S.E section, but fails in AVG.
Since our device only had a difference between Peak and AVG of 3 to 4 dBuV/m, we asked the certification company to measure it using CISPR.
However, I received a reply from the certification company that they only measure CISPR below 1GHz.
Please help.
thank you
Solved! Go to Solution.
2024-03-26 12:05 AM
Hello @danny92 and welcome to the ST Community :smiling_face_with_smiling_eyes:.
For such request, I suggest you contact your local Sales and marketing team or one of our FAEs. You can also submit a direct support ticket on our online Support platform.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-03-26 12:05 AM
Hello @danny92 and welcome to the ST Community :smiling_face_with_smiling_eyes:.
For such request, I suggest you contact your local Sales and marketing team or one of our FAEs. You can also submit a direct support ticket on our online Support platform.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-04-03 1:31 AM
Hello,
Yes, I will review it.
Thank you
Best Regards