2024-10-10 12:18 AM
Hi ,
I see in the Datasheet in Table 31 some reciever parameters .
I need to know what is the Dynamic Range of the Reciever in the STM32WLE5 . can you point me to which parameters should I look at ?
Thank you
Viola
2024-10-10 09:50 AM
Hello @viola
This depends on the RX sensitivity since it is the minimum signal level that the receiver can detect. But also, it depends on the position of the reception node, the used antenna, the electromagnetic interference that may happen due to the co-existence of different signals and finally the RF design.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.