cancel
Showing results for 
Search instead for 
Did you mean: 

Dynamic Range of STM32WLE5 RF reciever

viola
Associate III

Hi ,

 

I see in the Datasheet in Table 31 some reciever parameters .

I need to know what is the Dynamic Range of the Reciever in the STM32WLE5 . can you point me to which parameters should I look at ?

 

Thank you

Viola

1 ACCEPTED SOLUTION

Accepted Solutions
STTwo-32
ST Employee

Hello @viola 

This depends on the RX sensitivity since it is the minimum signal level that the receiver can detect. But also, it depends on the position of the reception node, the used antenna, the electromagnetic interference that may happen due to the co-existence of different signals and finally the RF design.

Best Regards.

STTwo-32 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

1 REPLY 1
STTwo-32
ST Employee

Hello @viola 

This depends on the RX sensitivity since it is the minimum signal level that the receiver can detect. But also, it depends on the position of the reception node, the used antenna, the electromagnetic interference that may happen due to the co-existence of different signals and finally the RF design.

Best Regards.

STTwo-32 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.