cancel
Showing results for 
Search instead for 
Did you mean: 

Does STM32WB55 have embedded pull-up resistor on USB_DP?

PLilj.1
Associate

In AN4879 FAQ it is stated to check "Table 3. USB implementation in STM32 devices" whether the USB_DP line has an embedded pull-up resistor.

STM32WB55 is not in that list. Can you confirm if the STM32WB55 has embedded pull-up resistor on USB_DP or not?

2 REPLIES 2
TDK
Guru

Per the reference manual, it has an embedded resistor on USB_DP.

USB connect / disconnect capability (controllable embedded pull-up resistor on USB_DP line)

If you feel a post has answered your question, please click "Accept as Solution".
垒垒.1
Associate II

YES!the STM32WB55 has embedded pull-up resistor on USB_DP.