2024-04-08 5:13 AM
I think I've spot a small bug into the cube mx code generation tool for STM_WPAN module
into app_debug.c in function
void DbgOutputTraces( uint8_t *p_data, uint16_t size, void (*cb)(void) )
{
/* USER CODE END DbgOutputTraces */
HW_UART_Transmit_DMA(CFG_DEBUG_TRACE_UART, p_data, size, cb);
/* USER CODE END DbgOutputTraces */
return;
}
There is 2 "END" tags the first one should be a BEGIN
due to this everything you wrote between both tag that should be kept when generating code from IOC file is scraped
thank's for the help
Solved! Go to Solution.
2024-05-02 1:36 AM - edited 2024-05-02 3:42 AM
Hello @oga
Thank you so much for reporting this. I've reported this issue to the concerned team for correction (under internal ticket number 180510).
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-05-02 1:36 AM - edited 2024-05-02 3:42 AM
Hello @oga
Thank you so much for reporting this. I've reported this issue to the concerned team for correction (under internal ticket number 180510).
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.