2021-05-01 8:56 PM
Hi,
I am a bit confused on the lora STM32WL sequence protocol system, I want my device to sleep and wakeup according to the periodic values I want. I have made my own sleep function (stop 2 mode & radio sleep) with wake up triggered using RTC (in seconds) and push button. Where can I put my function (PLB_SleepMode) into the sequencer utility lora end node STM32WL ?
Thank you
Here my code for custom sleep and wake up system:
void HAL_RTCEx_WakeUpTimerEventCallback(RTC_HandleTypeDef *RtcHandle)
{
//Clear wake up flag
__HAL_PWR_CLEAR_FLAG( PWR_FLAG_WU );
}
void PLB_RtcWakeUpTimeSetting( RTC_HandleTypeDef *RtcHandle, unsigned int seconds )
{
//Set wake up time
/* Disable all used wakeup source */
HAL_RTCEx_DeactivateWakeUpTimer( RtcHandle );
__HAL_RCC_WAKEUPSTOP_CLK_CONFIG( RCC_STOP_WAKEUPCLOCK_MSI );
HAL_RTCEx_SetWakeUpTimer_IT( RtcHandle, seconds - 1, RTC_WAKEUPCLOCK_CK_SPRE_16BITS );
}
RTC_HandleTypeDef *PLB_RtcPowerSavingConfig( void )
{
//Set RTC Clock, Timer, Calendar. and return RTC_HandleTypeDef to wake up
static RTC_HandleTypeDef RtcHandle;
RTC_TimeTypeDef sTime;
RTC_DateTypeDef sDate;
RtcHandle.Instance = RTC;
RtcHandle.Init.HourFormat = RTC_HOURFORMAT_24;
RtcHandle.Init.AsynchPrediv = 127;
RtcHandle.Init.SynchPrediv = 255;
RtcHandle.Init.OutPut = RTC_OUTPUT_DISABLE;
RtcHandle.Init.OutPutRemap = RTC_OUTPUT_REMAP_NONE;
RtcHandle.Init.OutPutPolarity = RTC_OUTPUT_POLARITY_HIGH;
RtcHandle.Init.OutPutType = RTC_OUTPUT_TYPE_OPENDRAIN;
HAL_RTC_Init( &RtcHandle );
sTime.Hours = 0x0;
sTime.Minutes = 0x0;
sTime.Seconds = 0x0;
sTime.TimeFormat = RTC_HOURFORMAT_24;
sTime.DayLightSaving = RTC_DAYLIGHTSAVING_NONE;
sTime.StoreOperation = RTC_STOREOPERATION_RESET;
HAL_RTC_SetTime( &RtcHandle, &sTime, FORMAT_BIN );
sDate.WeekDay = RTC_WEEKDAY_MONDAY;
sDate.Month = RTC_MONTH_JANUARY;
sDate.Date = 0x1;
sDate.Year = 16;
HAL_RTC_SetDate( &RtcHandle, &sDate, FORMAT_BIN );
return &RtcHandle;
}
void PLB_RtcRccPowerSavingConfig( void )
{
HAL_StatusTypeDef status = HAL_OK;
RCC_PeriphCLKInitTypeDef PeriphClkInit;
RCC_OscInitTypeDef RCC_OscInitStruct;
/* Disable backup domeain protection */
HAL_PWR_EnableBkUpAccess();
/* Enable RTC APB clock gating */
__HAL_RCC_RTCAPB_CLK_ENABLE();
/* Disable the Wake-up Timer */
__HAL_RTC_WAKEUPTIMER_DISABLE(RtcHandle);
/* In case of interrupt mode is used, the interrupt source must disabled */
__HAL_RTC_WAKEUPTIMER_DISABLE_IT(RtcHandle,RTC_IT_WUT);
__HAL_RTC_WAKEUPTIMER_CLEAR_FLAG(RtcHandle,RTC_FLAG_WUTF);
/* Get RTC clock configuration */
HAL_RCCEx_GetPeriphCLKConfig(&PeriphClkInit);
RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_LSE;
RCC_OscInitStruct.PLL.PLLState = RCC_PLL_NONE;
RCC_OscInitStruct.LSEState = RCC_LSE_ON;
PeriphClkInit.RTCClockSelection = RCC_RTCCLKSOURCE_LSE;
/* COnfigure oscillator */
status = HAL_RCC_OscConfig(&RCC_OscInitStruct);
if(status == HAL_OK)
{
/* Configure RTC clock source */
PeriphClkInit.PeriphClockSelection = RCC_PERIPHCLK_RTC;
status = HAL_RCCEx_PeriphCLKConfig(&PeriphClkInit);
/* Enable RTC Clock */
if(status == HAL_OK)
{
__HAL_RCC_RTC_ENABLE();
}
}
HAL_NVIC_EnableIRQ( RTC_WKUP_IRQn );
HAL_NVIC_SetPriority( RTC_WKUP_IRQn, 1, 0 );
}
void PLB_InitSystem(void)
{
HAL_Init();
PLB_SystemClock_Config( );
SystemApp_Init();
PLB_LED_Init(PLB_LED_MODE_RUN);
PLB_LED_Init(PLB_LED_LORA_INDICATOR);
PLB_LORA_Seq_Task();
}
void PLB_PowerSavingStopMode(RTC_HandleTypeDef *RtcHandle, unsigned int WakeUpTime, GPIO_TypeDef *WakeUpGPIO)
{
GPIO_InitTypeDef GPIO_InitStructure;
Radio.Sleep();
/* Enable GPIOs clock */
__HAL_RCC_GPIOA_CLK_ENABLE();
__HAL_RCC_GPIOB_CLK_ENABLE();
__HAL_RCC_GPIOC_CLK_ENABLE();
__HAL_RCC_GPIOH_CLK_ENABLE();
/* Configure all GPIO port pins in Analog Input mode (floating input trigger OFF) */
/* Note: Debug using ST-Link is not possible during the execution of this */
/* example because communication between ST-link and the device */
/* under test is done through UART. All GPIO pins are disabled (set */
/* to analog input mode) including UART I/O pins. */
GPIO_InitStructure.Pin = GPIO_PIN_All;
GPIO_InitStructure.Mode = GPIO_MODE_ANALOG;
GPIO_InitStructure.Pull = GPIO_NOPULL;
GPIO_InitStructure.Speed = GPIO_SPEED_FREQ_LOW;
HAL_GPIO_Init(GPIOA, &GPIO_InitStructure);
HAL_GPIO_Init(GPIOB, &GPIO_InitStructure);
HAL_GPIO_Init(GPIOC, &GPIO_InitStructure);
HAL_GPIO_Init(GPIOH, &GPIO_InitStructure);
//wake up pin setting
GPIO_InitStructure.Pin = PLB_WakeupPB_GPIO_Pin; // wakeup by PA.0
GPIO_InitStructure.Mode = GPIO_MODE_IT_RISING;
GPIO_InitStructure.Pull = GPIO_PULLDOWN;
GPIO_InitStructure.Speed = GPIO_SPEED_FREQ_HIGH;
HAL_GPIO_Init( GPIOA, &GPIO_InitStructure );
GPIO_InitStructure.Pin = GPIO_PIN_9;
GPIO_InitStructure.Mode = GPIO_MODE_OUTPUT_PP;
GPIO_InitStructure.Pull = GPIO_NOPULL;
GPIO_InitStructure.Speed = GPIO_SPEED_FREQ_VERY_HIGH;
HAL_GPIO_Init(GPIOA, &GPIO_InitStructure);
GPIO_InitStructure.Pin = GPIO_PIN_8;
HAL_GPIO_Init(GPIOA, &GPIO_InitStructure);
GPIO_InitStructure.Pin = GPIO_PIN_7;
HAL_GPIO_Init(GPIOA, &GPIO_InitStructure);
HAL_GPIO_WritePin(GPIOA, GPIO_PIN_8, GPIO_PIN_RESET);
HAL_GPIO_WritePin(GPIOA, GPIO_PIN_9, GPIO_PIN_RESET);
HAL_GPIO_WritePin(GPIOA, GPIO_PIN_7, GPIO_PIN_RESET);
HAL_NVIC_SetPriority(EXTI0_IRQn, 1, 0);
HAL_NVIC_EnableIRQ(EXTI0_IRQn);
/* Disable GPIOs clock */
__HAL_RCC_GPIOA_CLK_DISABLE();
__HAL_RCC_GPIOB_CLK_DISABLE();
__HAL_RCC_GPIOC_CLK_DISABLE();
__HAL_RCC_GPIOH_CLK_DISABLE();
//Set power saving duration by RTC
// if(WakeUpTime < 5 ) WakeUpTime = WakeUpTime + 5;
PLB_RtcWakeUpTimeSetting( RtcHandle, WakeUpTime );
// HAL_RTCEx_WakeUpTimerIRQHandler(RtcHandle);
HAL_PWR_EnableWakeUpPin(PWR_WAKEUP_PIN1);
//Clear wake up flag
if( __HAL_PWR_GET_FLAG( PWR_FLAG_WU ) != RESET )
{__HAL_PWR_CLEAR_FLAG( PWR_FLAG_WU ); }
if(__HAL_GPIO_EXTI_GET_FLAG(GPIO_PIN_0) != RESET)
{__HAL_GPIO_EXTI_CLEAR_FLAG(GPIO_PIN_0); }
/* Enter STOP 2 mode */
LL_PWR_ClearFlag_C1STOP_C1STB();
HAL_PWREx_EnterSTOP2Mode(PWR_STOPENTRY_WFI);
PLB_InitSystem();
Radio.Standby();
/*Disable all used wakeup sources: Pin1(PA.0)*/
HAL_PWR_DisableWakeUpPin(PWR_WAKEUP_PIN1);
}
void PLB_SleepMode(unsigned int wakeUpTime)
{
RTC_HandleTypeDef *RtcHandle;
APP_PRINTF("\nPowerSaving Mode - Start\n");
//RCC Config for Power Saving
PLB_RtcRccPowerSavingConfig();
//RTC Config for Power Saving
RtcHandle = PLB_RtcPowerSavingConfig();
//Enter Stop Mode
PLB_PowerSavingStopMode( RtcHandle, wakeUpTime, GPIOA );
APP_PRINTF("\nPowerSaving Mode - End\n");
}
Solved! Go to Solution.
2021-05-17 4:07 AM
2021-05-17 4:07 AM
2021-06-17 5:47 AM
Hello
i made a custom board using MIDATRONICS module that integrate the STM32WLE5J8I and i don't find how to make a lorawan end node project !!! when i import the end node project from the nucleo-WL package, it doesn't work (don't make a join and don't send data!!) and because the STM32WLE5J8I HAVE ONLY 64K of flash i'm at 96% of memory !!!
Can you help please ? is anybody make a lorawan end node project directly with cubeMX for the STM32WLE5J8I without any import from the Nucleo project?
Thank you in advance
Bests Regards
2021-06-17 5:57 AM
Hi @SHATE.1 ,
please open another question as this does not relate with question above.
thank you
2021-06-17 6:04 AM
Thank you for your quick reply
i asked a question " How we can made a LORAWAN End Node application with STM32WLE5J8I ????"
can you answer please?
Thank you in advance
2021-06-17 6:16 AM
Hi,
It is always good to check the .map file to check where to spend the optimization effort,
please find some tips:
back to my comment, the question you asked does not related to "Custom sleep and wakeup system on the lora end node STM32WL"
thank you and best regards