cancel
Showing results for 
Search instead for 
Did you mean: 

CUBEMX does not generate "hw_uart.c" when using the STM32_WPAN Peripheral

TomC
Senior

I believe that CUBEMX does not automatically generate the hw_uart.c file when trying to use the STM32_WPAN peripheral. I was following along with this tutorial and wished to use debug trace however it elicited the error undefined reference to `HW_UART_Transmit_DMA' as no implementation for the function existed.

In the example projects for the STM32WB available here, the hw_uart.c file is included.

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0