NUCLEO-WBA25CE1 "Bootloader limitation"
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link MATTER - Matter software expansion for STM32Cube - STMicroelectronics It is a reference implementation for the demonstration of Matter on ST...
Please go and visit our wiki pages where you can find a lot of information on our wireless product families (WB, WBA, WL) and the supported protocols: BLE, Zigbee, Thread, Matter, Lora, ... To begin your technical journey, please start from this top ...
I have a STM32WB55 Nucleo with which I would like to implement a BLE client (mast, central). In the end it should be able to automatically parse with another BLE (slave, peripheral). Currently I have no idea how to accomplish this task and my Google ...
Application note AN2606, on page 380. It says that in the default bootloader, USART is used on pin PA9 (E5)(TX) and PA10 (C8)(RX). However, when I select USART1 in STM32CubeMX, in mode Asynchronous, pins E1 (TX) and C3 (RX) are used. USART programmin...
Hi all, I'm trying to implement SPI TX communication with DMA. The following "prepareDMASPI()" function should configure and start DMA transferts from a buffer to the SPI device. But it doesn't work (No spi clock or MOSI data), although the SPI is pr...
Hi everyone,I am currently working on the STM32WL55JC, I am using the stm32cubewl_v1-1-0 for doing a LoRa application and a Sigfox application using the provided examples. I would like to know if there are any limitations (Hardware and/or software) f...
Good afternoon....Trying to trigger scan mode (2 channels but 3 conversions ---- A/D 9, A/D 9, A/D 10) via software trigger that is called in the LPTIMER (I do not have access to other timers bcz they are tied up in other code that is why I am not us...
Hi,we are working on an own hardware design with the STM32WL55.According to AN5457, section 5.1.2, I am supposed to select a Power mode (Low or High), and then a maximum output power for which I would want to optimize my design. With that maximum out...
My project involves LoRaWAN communication and embedded machine learning. we've trained a basic model which fits in flash memory, but barely. As our data set grows and our model becomes smarter, I imagine we will need more space. As of right now, our ...
I am running a scan mode of AD9 and AD10. I use a timer to generate an interrupt every 15ms....Inside this IRQ I start an ADC conversion scan.....After each conversion I store the value into an array. I have a potentiometer hooked up to adcValue[0] ....
Hi,I have a problem with USB CDC on STM32WB, after calling LL_C1_IPCC_SetFlag_CHx(IPCC, HW_IPCC_SYSTEM_CMD_RSP_CHANNEL). The USB stops working. Data cannot be sent or received via USB and also the USB IRQ is not working. The USB does not work also af...