cancel
Showing results for 
Search instead for 
Did you mean: 

Can't Download program to STM and stuck at FUS_FW_RUNNING

Aboyh
Associate II

STM32_Stuck_in_FUS.png

Hello mate,

I have a problem STM32WB55RG, i download BLE_p2pServer firmware to the board and success in stm32cubeide, but board can't run the firmware and i try download with stm32cubeprogrammer and i have same problem.

maybe someone can help me..

Thanks

5 REPLIES 5
STTwo-32
ST Employee

Hello @Aboyh 

This application requires having the stm32wb5x_BLE_Stack_full_fw.bin binary flashed on the Wireless Coprocessor (available here). So, please do a Stack update with this .bin. Then, start the wireless stack using the button "Start wireless stack" on the Cube Programmer interface:

STTwo32_1-1722934233881.png

Then, it should work fine.

Best Regards.

STTwo-32

 

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

I have tried it but the problem still occurs on my device

Wireless_STack.pngserial debug.png

Have you clicked on the button "Start Wireless Stack" after upgrading stack and firmware and before uploading your application. I think this is why you have this problem.

Best Regards

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

I have clicked on it

Could you please try another board. It should be working fine. 

Best Regards.

STTwo-32 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.