2024-08-06 01:00 AM
Hello mate,
I have a problem STM32WB55RG, i download BLE_p2pServer firmware to the board and success in stm32cubeide, but board can't run the firmware and i try download with stm32cubeprogrammer and i have same problem.
maybe someone can help me..
Thanks
2024-08-06 01:50 AM
Hello @Aboyh
This application requires having the stm32wb5x_BLE_Stack_full_fw.bin binary flashed on the Wireless Coprocessor (available here). So, please do a Stack update with this .bin. Then, start the wireless stack using the button "Start wireless stack" on the Cube Programmer interface:
Then, it should work fine.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.