I'm using a Stm32wb5mmgh6tr embbeded MCU for sharing data wireless via BLE. I just saw on the AN5185 application note document that wireless stack is not installed by default. So I've started FUS and then installed the latest version of the WS with STM32CubeProgrammer. After that, I've started the WS:
10:26:46 : Warning: Option Byte: nSWboot0, value: 0x0, was not modified. 10:26:46 : Warning: Option Byte: nboot0, value: 0x1, was not modified. 10:26:46 : Warning: Option Byte: nboot1, value: 0x1, was not modified. 10:26:46 : Warning: Option Bytes are unchanged, Data won't be downloaded 10:26:46 : Time elapsed during option Bytes configuration: 00:00:00.003 10:26:46 : Succeeded to set nSWboot0=0 nboot1=1 nboot0=1 10:26:46 : Memory Programming ... 10:26:46 : Opening and parsing file: 0x495_FUS_Operator.bin 10:26:46 : File : 0x495_FUS_Operator.bin 10:26:46 : Size : 8.00 KB 10:26:46 : Address : 0x08000000 10:26:46 : Erasing memory corresponding to segment 0: 10:26:46 : Erasing internal memory sectors [0 1] 10:26:46 : Download in Progress: 10:26:46 : File download complete 10:26:46 : Time elapsed during download operation: 00:00:00.292 10:26:46 : Application is running, Please Hold on... 10:26:47 : Reconnecting... 10:26:47 : Reconnected ! 10:26:48 : FusStartWS activated successfully 10:26:48 : Warning: Option Byte: nSWboot0, value: 0x0, was not modified. 10:26:48 : Warning: Option Byte: nboot0, value: 0x1, was not modified. 10:26:48 : Warning: Option Byte: nboot1, value: 0x1, was not modified. 10:26:48 : Warning: Option Bytes are unchanged, Data won't be downloaded 10:26:48 : Time elapsed during option Bytes configuration: 00:00:00.000 10:26:48 : Succeeded to set nSWboot0=0 nboot1=1 nboot0=1 10:26:48 : Memory Programming ... 10:26:48 : Opening and parsing file: 0x495_FUS_Operator.bin 10:26:48 : File : 0x495_FUS_Operator.bin 10:26:48 : Size : 8.00 KB 10:26:48 : Address : 0x08000000 10:26:48 : Erasing memory corresponding to segment 0: 10:26:48 : Erasing internal memory sectors [0 1] 10:26:48 : Download in Progress: 10:26:48 : File download complete 10:26:48 : Time elapsed during download operation: 00:00:00.271 10:26:48 : Application is running, Please Hold on... 10:26:49 : Reconnecting... 10:26:50 : Reconnected ! 10:26:51 : FusStartWS activated successfully 10:26:51 : Start Wireless Stack command execution finished with success
And I've downloaded BLESensor binary example but it seems that BLE isn't starting since I can't see the BLE device in my phone.
I've checked SBRV Option Bytes value and it's 0x33800, which corresposts to FUS not running. Also I've included here some screenshots of the ST-Link config and FUS version.