2025-01-24 3:02 AM - edited 2025-01-24 3:04 AM
Hello,
I designed my custom board using STM32WB series to be connected to sensor and send data to CLIENT which is my laptop. I am able to use Write and Read Characteristics for a single character.
Now I intend to use READ characteristic to send data every 5 millisecond to laptop. My sensor data payload can be maximum 120 Bytes.
Do you see any issues here on STM32WB ? Does BLE support this much ?
2025-01-24 3:09 AM
@Nico3 wrote:I intend to use READ characteristic to send data every 5 millisecond
Does it really need to be that fast?
As well as the the STM32, you have to consider the PC end - it may not allow such fast updates...
2025-01-24 3:31 AM
I was wondering the same, i dont think Host PC can handle that rate.
In the other hand, i am able to transfer up to 512 bytes per window using BLE. But i never tryed as a constant way to update but more like "when" some variable suffer a change in the "server" i make a "notifcation" to update that value in the paired client. At the end BLE is not like UART, in BLE you have characteristics and they should be used for particular scenarios.
2025-01-24 3:44 AM
@urbito wrote:I was wondering the same, i dont think Host PC can handle that rate.
It's not so much that it can't handle it - just that it may not allow it.
Windows decides how it allocates the radio resources.
Similarly on phones/tablets.
You didn't if it really needs to be that fast?
2025-01-24 4:09 AM
I am data logging vibration data from multiple sensors. I need vibration data atleast of 10Hz frequency. So I need to sample atleast at 20Hz. That means data logging every 50 ms.
I am thinking to go higher as much possible so data FFT is more reliable. If 5ms is too much, then i go for 20 or last 50 ms.
2025-01-24 4:10 AM
Arent you able to hold that data in host MCU for 500ms and then send it to Client PC? For example...
2025-01-24 4:12 AM
yes,,this can be workable... never came to my mind..
2025-01-24 4:13 AM
Then try to give it a shoot :)
Hopefully it helps!
Greetings