2019-09-04 12:29 AM
Hi,
I wanted to generate PWM using timer on B-L072Z-LRWAN1 board for LED Dimming.
I searched on the forum and web for this but I am unable to get any example for PWM on B-L072Z-LRWAN1 .
Which LED I can use for this purpose?
Can any one help me with this?
2019-09-04 2:47 AM
Brain is for thinking!
AN4013 and AN4776 are good helpers for this task.
2019-09-04 4:12 AM
void pwm_setvalue(uint16_t value)
{
TIM_OC_InitTypeDef sConfigOC;
sConfigOC.OCMode = TIM_OCMODE_PWM2;
sConfigOC.Pulse = value;
sConfigOC.OCPolarity = TIM_OCPOLARITY_HIGH;
sConfigOC.OCFastMode = TIM_OCFAST_DISABLE;
HAL_TIM_PWM_ConfigChannel(&TimHandle, &sConfigOC, TIM_CHANNEL_1);
HAL_TIM_PWM_Start(&TimHandle, TIM_CHANNEL_1);
}
void timer21_init(void)
{
TimHandle.Instance = TIM21;
TimHandle.Init.Prescaler = 0;
TimHandle.Init.CounterMode = TIM_COUNTERMODE_UP;
TimHandle.Init.Period = 3000;
TimHandle.Init.ClockDivision = TIM_CLOCKDIVISION_DIV1;
HAL_TIM_PWM_Init(&TimHandle);
}
void gpio_tim_init(void)
{
/* Enable the GPIO_LED Clock */
__HAL_RCC_GPIOA_CLK_ENABLE();
/* Configure the GPIO_LED pin */
GPIO_InitStruct.Pin = GPIO_PIN_13;
GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_HIGH;
GPIO_InitStruct.Alternate = GPIO_AF6_TIM21;
//HAL_TIM_PWM_Start(&TimHandle, TIM_CHANNEL_1);
HAL_GPIO_Init(GPIOB, &GPIO_InitStruct);
}
int main( void )
{
HAL_Init( );
SystemClock_Config( );
HW_Init( );
gpio_tim_init();
timer21_init();
while(1)
{
HAL_Delay(100);
if(pwm_value == 0)
{
step = 100;
}
if(pwm_value == 3000)
{
step = -100;
}
pwm_value += step;
pwm_setvalue(799);
}
Could u tell me what's wrong in this code because I am not getting PWM on pin PB13.