cancel
Showing results for 
Search instead for 
Did you mean: 

X-NUCLEO-GFX01M2 has color display or mono chrome?

mdalal
Associate III

Hi,

 

Can you confirm if the X-NUCLEO-GFX01M2 has a color display or monochrome display? 

1 ACCEPTED SOLUTION

Accepted Solutions

It's a colour display

6.2 X-NUCLEO-GFX01M1 product history 6.2.1 Product identification XNGFX01M1$AZ1 This product identification is based on board MB1642-DT022CTFT-B01. The LCD used in this product is DT022CTFT with driver IC ILI9341V. Product limitations No limitation identified for this product identification. 6.3 X-NUCLEO-GFX01M2 product history 6.3.1 Product identification XNGFX01M2$AZ1 This product identification is based on board MB1642-TCXD022IB5-D01. The LCD used in this product is TCXD022IBLON-5 with driver IC ST7789V. Product limitations No limitation identified for this product identification. 6.3.2 Product identification XNGFX01M2$AZ2 This product identification is based on board MB1642-DT022CTFT-D01. The LCD used in this product is DT022CTFT with driver IC ILI9341V.

https://community.st.com/t5/stm32-mcus-touchgfx-and-gui/need-datasheet-for-lcd-display-xinli-pn-tcxd022iblon-5-used-on-x/td-p/89486

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

View solution in original post

4 REPLIES 4
mdalal
Associate III

Since it is QVGA, I assume it supports color but the datasheet is not specifying anything on it so just want to confirm.

It's a colour display

6.2 X-NUCLEO-GFX01M1 product history 6.2.1 Product identification XNGFX01M1$AZ1 This product identification is based on board MB1642-DT022CTFT-B01. The LCD used in this product is DT022CTFT with driver IC ILI9341V. Product limitations No limitation identified for this product identification. 6.3 X-NUCLEO-GFX01M2 product history 6.3.1 Product identification XNGFX01M2$AZ1 This product identification is based on board MB1642-TCXD022IB5-D01. The LCD used in this product is TCXD022IBLON-5 with driver IC ST7789V. Product limitations No limitation identified for this product identification. 6.3.2 Product identification XNGFX01M2$AZ2 This product identification is based on board MB1642-DT022CTFT-D01. The LCD used in this product is DT022CTFT with driver IC ILI9341V.

https://community.st.com/t5/stm32-mcus-touchgfx-and-gui/need-datasheet-for-lcd-display-xinli-pn-tcxd022iblon-5-used-on-x/td-p/89486

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

Thanks.

Can you suggest if there is any exmasion board for STM32 Nucleo-64 which has a monochrome display?

Billy OWEN
ST Employee

Hi @mdalal 

 

This post has been escalated to the ST Online Support Team for additional assistance.  We'll contact you directly.

 

Regards,

Billy