2024-06-30 2:37 AM
Hello
I am using a Mac. There is software support for stm32cude ide on Mac. But I would like to ask if there is support for Touchgfx application on a Mac.
On the website https://www.st.com/en/embedded-software/x-cube-touchgfx.html
I can not find a link to download the software for Mac.
Is there software support for Mac or any other way to run this application?
Thank you
Solved! Go to Solution.
2024-07-02 2:39 AM
Hello @Avgerinos ,
There is no support for TouchGFX on macOS.
However, there is still 2 ways you can use TouchGFX on your Apple computer:
If this comment answers your question, I invite you to select it as "best answer".
Regards,
2024-07-02 2:39 AM
Hello @Avgerinos ,
There is no support for TouchGFX on macOS.
However, there is still 2 ways you can use TouchGFX on your Apple computer:
If this comment answers your question, I invite you to select it as "best answer".
Regards,
2024-07-02 8:09 AM
Hello
Is there a plan for Mac support in the near future?
Thank you for your answer
2024-07-04 12:23 AM
Hello @Avgerinos ,
Not in the near future but we are thinking about it!
Regards,
2025-03-13 8:15 AM
I do own a M3 MacBook Pro and can't dual boot into Windows. Do you have any other options, beside a second laptop or a virtual machine (which slows down development)?
2025-03-28 11:36 AM
In the beginning, STM32CubeMX only ran on Windows and Linux, but someone figured out that it was all just a big Java program and figured out that it ran perfectly well on Mac if you just pointed Java at the .jar file. Word eventually got out and within a reasonable time period ST started officially supporting Cube on Mac.
I have not tried this with TouchGFX, as I still have a few Intel Macs around that I use with Fusion.
2025-03-28 1:01 PM
TouchGFX is not based on Java, so it is not so easy to make it run under MacOSX. But at least you can get on with VMWare Fusion.