cancel
Showing results for 
Search instead for 
Did you mean: 

Wrong colors with TouchGFX 4.18.0

Andrew1
Associate II

Steps to reproduce issue:

Create new project in TouchGFX 4.18.0, set target board H743 eval, add box with border, set border color to red, box color to green, save project, generate code, build and download to board with CubeIDE

1 ACCEPTED SOLUTION

Accepted Solutions
Romain DIELEMAN
ST Employee

Hi,

Could you try to open re generate code from STM32CubeMX first and then running on target from TouchGFX Designer ?

/Romain

View solution in original post

4 REPLIES 4
Romain DIELEMAN
ST Employee

Hi,

Could you try to open re generate code from STM32CubeMX first and then running on target from TouchGFX Designer ?

/Romain

Andrew1
Associate II

Thank you, after generating code with STM32CubeMX 6.3.0 colors are correct

Guit32010
Associate III

I am having the same problem. However, i no longer have a cube file associated with my project, so I can't easily regenerate the files. Do you know which specific files need upgrading? Or is there an easy way to link a cube file into the project and prevent it from writing over any user code in the process?

Guit32010
Associate III

I figured it out. I created a new TGFX designer project with the same MCU. then copied the STM32DMA files to my other project.