cancel
Showing results for 
Search instead for 
Did you mean: 

Why is the UI display on my screen distorting?

Junde
Senior III

Hi,

I have tried many times to configure touchGFX with cubeMx, and I was finally almost successful. My screen is 1024*600, and the driver chip is EK79001.

Now the widgets shown on display are distorting(the image seems right), as below:

0693W00000aJs4xQAC.jpgBut my designer is the following:0693W00000aJs57QAC.jpgthe LTDC parameters and the datasheet are as below:

0693W00000aJs5lQAC.png0693W00000aJs6KQAS.pngI really don't know, why this happened, could you help me?

Thanks a lot.

10 REPLIES 10

@Community member​ 

Thanks for such a detailed explanation.

I already try to display 2 squares (just 2 boxes, nothing updated), but the display is also distorting.

I think changing the color format to L8 from RGB565 is a good try.

Anyway, I will tell you the latest result.

Thanks again and have a good weekend.