2020-01-03 06:08 AM
Where is STMCubeMX v5.5.0?
...or...
How do I get STM32CubeMX to download a version of TouchGFX that it is compatible with?
Cheers,
Murray
Solved! Go to Solution.
2020-01-06 02:04 AM
We'll unveil the exact reason for the X-CUBE not being compatible with CubeMX 5.4.0. There's no more TouchGFX Middleware in CubeMX - It's being replaced by "TouchGFX Generator" add-on which now generates your TouchGFX HAL. It feeds the designer input like screen dimensions (=> canvas dimensions) and bitdepth.
/Martin
2020-01-07 12:48 PM
Hi,
STM32CubeMX 5.5.0 is availble for donwload (https://www.st.com/en/development-tools/stm32cubemx.html) or direct upgrade of your existing install.
Regards
Jérôme
2020-01-07 06:46 PM
So this new 5.5.0 shows it is RC6 dated 12-30-2019 and the 5.5.0 that i got from ST support is dated 12-20-2019. They both show an error as shown in the image. I have tried different combinations using the drop downs but i can't get rid of the error which prevents me from generating a project. How do you start TouchGFX from CubeMX? I have both TouchGFX 4.12.3 and 4.13.0 installed. What am i doing wrong?
2020-01-08 03:58 AM
It's not an error. It's a warning to say that you do not need this particular blending factor for your LTDC layer.
2020-01-08 03:58 AM
Did you read the post i made with links to articles on both installation and use of the generator?
https://community.st.com/s/question/0D50X0000BwjU6pSQE/official-release-xcubetouchgfx-v4130
2020-01-08 04:03 AM
Could you please create a new post titled with any specific issue you may have? I'm closing this as the question was already answered by Jerome.