Why does model::tick() not getting called?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2022-10-02 11:59 PM
I found out that LTDC interupt callback is not getting called but can't figure why.
Following code is auto generated by CubeMX LTDC interrupt is enabled in NVIC.
"TouchGFXGeneratedHAL.cpp"
extern "C"
{
void HAL_LTDC_LineEventCallback(LTDC_HandleTypeDef* hltdc)
{
if (!HAL::getInstance())
{
return;
}
if (LTDC->LIPCR == lcd_int_active_line)
{
//entering active area
HAL_LTDC_ProgramLineEvent(hltdc, lcd_int_porch_line);
HAL::getInstance()->vSync();
OSWrappers::signalVSync();
// Swap frame buffers immediately instead of waiting for the task to be scheduled in.
// Note: task will also swap when it wakes up, but that operation is guarded and will not have
// any effect if already swapped.
HAL::getInstance()->swapFrameBuffers();
GPIO::set(GPIO::VSYNC_FREQ);
}
else
{
//exiting active area
HAL_LTDC_ProgramLineEvent(hltdc, lcd_int_active_line);
// Signal to the framework that display update has finished.
HAL::getInstance()->frontPorchEntered();
GPIO::clear(GPIO::VSYNC_FREQ);
}
}
}
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2022-10-20 10:51 AM
Hi,
There could be several reasons for that but more information is needed here.
First, what is your STM32 ? Have you compared your code with the Board Setup of the closest MCU ?
Could you please specify your display definition, a well as the LTDC frequency you set ?
Do you reach the TouchGFXGeneratedHAL::enableInterrupts() call ?
If not, do you pass the TouchGFXGeneratedHAL::initialize() call successfully ?
What about LTDC registers ? Do you see the interrupts enabled in IER register ?
Could you maybe share more of your project in not all, notably the main.c (with LTDC init, ltdc.c otherwise) and full TouchGFXGenerated.cpp, TouchHAL.cpp and TouchGFXConfiguration.cpp ?
Best regards,
Nicolas