cancel
Showing results for 
Search instead for 
Did you mean: 

who has some example of how to connect l�?d spi interface with touchgfx?

Lviet.1
Associate II
 
This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Romain DIELEMAN
ST Employee

Hi,

The application template for the STM32G0 board available in TouchGFX may help you, it has an SPI display. When you will create a project with this application template or with one of the corresponding online application, a fully configured project will be generated and can be used as a source of inspiration.

These two articles in the documentation may help you as well: "partial frame buffer with SPI" and "FMC and SPI display interfaces"

/Romain

View solution in original post

2 REPLIES 2
Imen GH
ST Employee
Romain DIELEMAN
ST Employee

Hi,

The application template for the STM32G0 board available in TouchGFX may help you, it has an SPI display. When you will create a project with this application template or with one of the corresponding online application, a fully configured project will be generated and can be used as a source of inspiration.

These two articles in the documentation may help you as well: "partial frame buffer with SPI" and "FMC and SPI display interfaces"

/Romain