2021-03-02 11:48 PM
2021-03-03 3:27 AM
Hi,
The application template for the STM32G0 board available in TouchGFX may help you, it has an SPI display. When you will create a project with this application template or with one of the corresponding online application, a fully configured project will be generated and can be used as a source of inspiration.
These two articles in the documentation may help you as well: "partial frame buffer with SPI" and "FMC and SPI display interfaces"
/Romain
2021-03-03 3:18 AM
Hello @Lviet.1 ,
I share with you this discussion:
https://community.st.com/s/question/0D53W00000IrpnnSAB/touchgfx-video-tutorial-step-by-step-to-interface-with-spi-lcd-or-with-fsmc-interface
it may be can help you
Imen
2021-03-03 3:27 AM
Hi,
The application template for the STM32G0 board available in TouchGFX may help you, it has an SPI display. When you will create a project with this application template or with one of the corresponding online application, a fully configured project will be generated and can be used as a source of inspiration.
These two articles in the documentation may help you as well: "partial frame buffer with SPI" and "FMC and SPI display interfaces"
/Romain