cancel
Showing results for 
Search instead for 
Did you mean: 

Which widget can be used to drag up and down in video

bli.1
Associate II

1�?Used in smartWatch .

2�?Which widgetcan be used to drag up and down in video

1 ACCEPTED SOLUTION

Accepted Solutions
Romain DIELEMAN
ST Employee

Hi :beaming_face_with_smiling_eyes:,

There are multiple way to do this depending on what you want to acheive. A widget you could use would be the SlideMenu widget.

You could also adapt the swipeContainer widget to have a vertical scroll instead of a horizontal scroll.

Have a look at the documentation to understand how to work with TouchGFX and the different widgets available. You can download the different UI templates and demos to look at the code and use it as source of inspiration :beaming_face_with_smiling_eyes:​

/Romain

View solution in original post

4 REPLIES 4
bli.1
Associate II

:beaming_face_with_smiling_eyes:

bli.1
Associate II

help​

Romain DIELEMAN
ST Employee

Hi :beaming_face_with_smiling_eyes:,

There are multiple way to do this depending on what you want to acheive. A widget you could use would be the SlideMenu widget.

You could also adapt the swipeContainer widget to have a vertical scroll instead of a horizontal scroll.

Have a look at the documentation to understand how to work with TouchGFX and the different widgets available. You can download the different UI templates and demos to look at the code and use it as source of inspiration :beaming_face_with_smiling_eyes:​

/Romain

bli.1
Associate II

Your advice is great�?thanks you!:grinning_face: