2022-05-31 9:12 PM
The TFT dsiplay was cracked, can I but the display only from ST ?
Solved! Go to Solution.
2022-05-31 11:37 PM
Hello @Lemuel,
Of course you can buy it separately, here for example.
Also, that question doesn't concern TouchGFX, so please try to change or add more tags next time you are creating a new post please ;)
Hope that it helped you,
/Yoann
2022-05-31 11:37 PM
Hello @Lemuel,
Of course you can buy it separately, here for example.
Also, that question doesn't concern TouchGFX, so please try to change or add more tags next time you are creating a new post please ;)
Hope that it helped you,
/Yoann
2022-06-01 12:10 AM
The display can also be bought separately from Mouser or Digikey, for example, but it is only slightly cheaper than the complete X-NUCLEO-GFX01M2. That's why @Yoann KLEIN suggested the URL to buy a complete X-NUCLEO, which is definitely the easiest option.
Good luck!
Regards
/Peter
2022-06-01 2:28 AM
Peter and Yoann,
Thanks for your advice.
Yes, the screen from Mouser and Digikey is quite expensive either, I can't afford that.:loudly_crying_face:
May be I try my luck in taobao and alibaba too.
Best regards,
Fai
2022-06-01 12:47 PM
DISPLAYTECH DT022CTFT
https://www.seacomp.com/product/2-2-inch-tft-lcd-dt022ctft