Solved
Howto combine TouchGFX and WPAN BLE ?
Project MX created without RTOS generate this main part
MX_TouchGFX_Init();
MX_RTC_Init();
/* USER CODE BEGIN 2 */
/* USER CODE END 2 */
/* Init code for STM32_WPAN */
MX_APPE_Init();
/* Infinite loop */
/* USER CODE BEGIN WHILE */
while (1)
{
/* USER CODE END WHILE */
MX_APPE_Process();
MX_TouchGFX_Process();
/* USER CODE BEGIN 3 */
if((HAL_GPIO_ReadPin(TOUCH_IRQ_GPIO_Port,TOUCH_IRQ_Pin) == GPIO_PIN_RESET ||
i2cRXbuff[0]!=0) && TouchDELAY==0)
if (HAL_I2C_Master_Transmit(&hi2c1, 0x5c, (uint8_t *)"\340", 1, 1) == HAL_OK)
{
TouchDELAY=14;
HAL_I2C_Master_Receive_IT(&hi2c1, 0x5c, i2cRXbuff, 5);
}
}
/* USER CODE END 3 */If i comment RTC and APPE = TouchgfX works.
If TouchGFX commented BLE works.
Is BLE RTOS compliant? Or how add (move) TouchGFX_Process into sequencer?