2024-08-05 03:14 AM - last edited on 2024-08-05 03:18 AM by Andrew Neil
Hello,
I'm currently learning how to use an STM32H7B3I-EVAL, I'm just starting out. I'm trying to debug a simple TouchGFX project with only a slider with STM32CubeIDE.
The problem is that when debugging I get a warning:
Warning: the current language does not match this frame.
set *(int *)0xE000EDFC=*(int *)0xE000EDFC|0x7F0
I use : TouchGFX 4.20
CubeIDE 1.9
Does anyone have an explication please?
Solved! Go to Solution.
2024-08-09 04:48 AM
Yes, Swipe Container has a member function called getSelectedPage() that returns the page that is currently displayed.
You can use handleDragEvent(const DragEvent& Event) to detect when the container is swiped, so you can change your text. For instance:
void Screen1View::handleDragEvent(const DragEvent& Event)
{
Screen1ViewBase::handleDragEvent(Event);
uint8_t pageNumber = swipeContainer.getSelectedPage();
switch (pageNumber)
{
case 0:
//Update the text for the first page
break;
case 1:
//Update the text for the second page
break;
case 2:
//Update the text for the thrid page
break;
default:
break;
}
}
I hope this helps you!
2024-08-06 06:14 AM
Hello @rozeelc,
I tried to replicate the project you have, but I didn't encounter the issue you mentioned.
Are you using the available TouchGFX Board Setup (TBS) for STM32H7B3I-Eval?
TBS for STM32H7B3I-Eval
I also noticed that in your debugger, no External Loader is selected. Do you still manage to start the debugger?
2024-08-07 05:25 AM - edited 2024-08-07 05:27 AM
Hello @Mohammad MORADI ESFAHANIASL ,
I'm sorry for the inconvenience. I managed to resolve the initial problem by selecting an External Loader. However, I now have another question and I hope you can help me.
I apologize if there are any errors, I am French.
I am working on creating a mixing console with 512 sliders. I have created a page with 8 sliders, and it is necessary to swipe to switch from one set of sliders to another. Above each slider, I want to display its value. My problem is that to display the value of the slider, I have to create a new interaction for each one.
I would like to know if TouchGFX can handle more than 512 interactions and if there is a simpler way to achieve what I want.
Thank you in advance for your help.
2024-08-07 05:50 AM
I'm glad you fixed the first issue :D
To have a better architecture for your GUI, I suggest creating a Custom Container that contains the slider and a text area to show its value, then you can easily control the interactions inside the container.
Then, you can place your custom container instances inside a Swipe Container to accommodate all of them in a container that supports multiple pages.
I hope this helps you achieve what you need.
2024-08-07 06:55 AM - edited 2024-08-07 06:55 AM
Thank you very much @Mohammad MORADI ESFAHANIASL for your help.
I don't see how to use the container to manage the slider and the variable. If I use a container I don't need interactions anymore? How can I use a container to change my variable according to my slider?
I'm sorry for all my questions, this is the first time I've used TouchGFX.
2024-08-08 02:18 AM
You're very welcome!
There are plenty of helpful materials such as tutorials and videos that teach about TouchGFX in the TouchGFX Academy.
Please refer to them especially Tutorial 4 and Tutorial 5, as they use Custom Containers.
Best regards,
2024-08-08 06:11 AM
Hello,
thank you for your answer, it helped me a lot.
I have another question. Do you know how to get the current page from "swipcontainer" so that I can change the text according to the current page?
Thank you in advance.
Best regards,
2024-08-09 04:48 AM
Yes, Swipe Container has a member function called getSelectedPage() that returns the page that is currently displayed.
You can use handleDragEvent(const DragEvent& Event) to detect when the container is swiped, so you can change your text. For instance:
void Screen1View::handleDragEvent(const DragEvent& Event)
{
Screen1ViewBase::handleDragEvent(Event);
uint8_t pageNumber = swipeContainer.getSelectedPage();
switch (pageNumber)
{
case 0:
//Update the text for the first page
break;
case 1:
//Update the text for the second page
break;
case 2:
//Update the text for the thrid page
break;
default:
break;
}
}
I hope this helps you!
2024-08-12 12:19 AM - edited 2024-08-12 05:44 AM
Thank you for your help.
Do you know if there is a page limit with Swipecontainer? I'm stuck at 53 pages but I need to make 64.
Best regards,
2024-08-14 02:33 AM
You're very welcome,
There is no limit for the number of pages for the Swipe Container. What do you mean by 'being stuck at 53 pages'?