cancel
Showing results for 
Search instead for 
Did you mean: 

Unable to compile and run my simulator (static const touchgfx::FontId HUGE = 2; issue)

louiev
Associate

I get the following error every I try to to run my simulator.  The same generated code is compiling fine on my target.

I keep getting an error related to static const touchgfx::FontId HUGE = 2;.

Compiling gui/src/pages/views/SettingsCommunicationView.cpp
In file included from C:/TouchGFX/4.24.2/env/MinGW/i686-w64-mingw32/include/_mingw.h:12:0,
from C:/TouchGFX/4.24.2/env/MinGW/i686-w64-mingw32/include/crtdefs.h:10,
from C:/TouchGFX/4.24.2/env/MinGW/i686-w64-mingw32/include/assert.h:15,
from ../Middlewares/ST/touchgfx/framework/include/touchgfx/hal/Types.hpp:22,
from ../Middlewares/ST/touchgfx/framework/include/touchgfx/canvas_widget_renderer/Cell.hpp:21,
from ../Middlewares/ST/touchgfx/framework/include/touchgfx/canvas_widget_renderer/CanvasWidgetRenderer.hpp:21,
from gui/src/main_screen/MainView.cpp:1:
generated/fonts/include/fonts/ApplicationFontProvider.hpp:18:35: error: 'constexpr' needed for in-class initialization of static data member 'const FontId* Typography::_imp___HUGE' of non-integral type [-fpermissive]
static const touchgfx::FontId HUGE = 2;

Please help.

2 REPLIES 2
MM..1
Chief III

Maybe HUGE isnt right name ...

ApplicationFontProvider.hpp is a generated file and HUGE is something it used.