cancel
Showing results for 
Search instead for 
Did you mean: 

Trivial question about customizing a keyboard

Mvill.17
Associate III

I redesign a layout of a keyboad (as I'm interested in numeric keys only, for a login).

Everything is OK but I didn't managed to place the text of the key inside its button shape

( i.e. texts: "1", "2", etc appears outside the button)

How can I tell where to draw the texts of keys?

Thanks

2 REPLIES 2
Romain DIELEMAN
ST Employee

Hi,

What have you done exactly ? Are you using the keyboard example provided in TouchGFX Designer or a project of your own ?

Could you share some screenshots or some code ?

/Romain

Mvill.17
Associate III

I solved the problem in another way: I redesigned the layout from the ground up and wrote a class to handle my custom keyboard but it was a pity

having a working framework which already handles a quite generic layout and give up just because the keys text appear not centerd respect to the keys itselves.

Anyway the original layout was: