2020-12-09 3:51 PM
I'm using a ToughGFX Designer with STM32H7B3I-DK and when I hit "Run Target" it runs but then stops with the error below. How do I fix it?
Erasing memory corresponding to segment 1:
Erasing memory corresponding to segment 2:
Download in Progress:
±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±± 0%
ÛÛÛÛÛÛÛÛÛÛÛÛÛÛÛÛÛÛÛÛÛÛÛÛÛÛÛÛÛÛÛÛÛÛÛÛÛ 75%ÛÛÛÛÛÛÛÛÛÛÛÛÛÛÛÛÛÛÛÛÛÛÛÛÛÛÛÛ 69%ÛÛÛÛÛÛÛÛÛÛÛÛÛÛÛÛ 100%
Error: failed to download Segment[2]
Error: failed to download the File
Hard reset is performed
gcc/Makefile:294: recipe for target '_extflash_' failed
make[1]: *** [_extflash_] Error 1
../gcc/Makefile:52: recipe for target 'flash' failed
make: *** [flash] Error 2
Failed
Failed
Solved! Go to Solution.
2020-12-09 7:44 PM
It could be the Cubeprogrammer 2.6, please use 2.5 instead.
https://community.st.com/s/question/0D53W00000O1KHJSA3/run-target-on-stm32h747idisco-failed
2020-12-09 6:46 PM
Hello,
First could you try to open TouchGFX Designer 4.15, use the Application Template for H7B3-DK as well as the Animated Image Example, then Generate Code and Run Target ?
Do you still have the issue ?
If yes, please provide more information to understand the cause of the download error. Also, provide your board serial number.
/Alexandre
2020-12-09 7:44 PM
It could be the Cubeprogrammer 2.6, please use 2.5 instead.
https://community.st.com/s/question/0D53W00000O1KHJSA3/run-target-on-stm32h747idisco-failed
2020-12-10 2:12 PM
Thanks victagayun. I installed Cubeprogrammer 2.6 and it worked